How can we help?

am getting repeated errors in the app that prevent me from completing advanced setup of my controller, what should I do?

Some button clicks do not match your remote When setting up the product, Smarther will receive infrared commands from your remote control when you click the buttons. If other infrared products are nearby, it may cause interference and result in repeated errors during advanced setup. To avoid these errors, follow these suggestions: - Move away from other products that use infrared (TV remote control, motion sensor on lights, etc.). - Make sure your smartphone is not too close to your Smarther (about 1 meter) and that it is not between your air conditioner remote control and Smarther. Some smartphone features, such as facial recognition, may cause interference. If the error persists despite checking the compatibility of your remote control (check.netatmo.com), send us a message with a photo of your remote control (front and back). My product does not beep? During setup, Smarther beeps to confirm that it has received a command from the remote control. If you do not hear this beep, Smarther is not configured correctly. Check the following: - Make sure the remote control batteries are full and that the remote control can control your air conditioner. - Make sure the remote control works. - Point the remote control at the Smarther from less than one meter away. If you still do not hear a beep after performing these checks, please follow these steps: 1. Unplug the Smarther and apply power. Wait a few seconds, then start the setup from the product settings: Menu > Manage my home > Room selection > Configure my remote 2. If step 1 does not work, please reset and reinstall your product. To do this: - Remove your product from Home + Control: Manage my home > Room > Smarther > Settings > Delete - Reset the product by pressing the bottom right button for 5 seconds until you hear a beep - Reinstall the product