How can we help?

Can't I configure the built-in IR transmitter on my Smarther air conditioner with Netatmo if I don't need it (example: configuration with additional IR transmitters controlled via Zigbee)?

The built-in IR on the Smarther AC with Netatmo device can be disabled or used in parallel with an additional IR transmitter to control an additional air conditioner. If you don't need it, you can skip its configuration during commissioning.