How can we help?

I'm experiencing recurring errors in the app that prevent me from completing my controller's advanced setup. What should I do?

The beeps do not correspond to your remote control. During product setup, the Smarther AC will receive commands from your remote control when you press buttons. If other infrared products are nearby, this may cause interference and lead to recurring errors during advanced setup. To avoid these errors, follow these recommendations: - Move away from other products that use infrared (TV remote control, motion sensor on lighting, etc.). - Make sure your smartphone is not too close to your Smarther AC (about 1 meter) and that it is not between your air conditioner remote control and the Smarther AC. Some smartphone features such as facial recognition may cause interference. If the error persists despite checking the compatibility of your remote control (check.netatmo.com), please send us a message with a photo (front and back) of your remote control. My product does not beep? During installation, the Smarther AC beeps to confirm that it has received a command from your remote control. If you do not hear the beep, the Smarther AC cannot be configured correctly. Please check the following: - Make sure the batteries in the remote control are new and that the remote control can control your air conditioner. - Make sure the remote control is turned on Point the remote control at the Smarther AC, within a distance of less than 1 meter. If you still do not hear the beep after these steps, follow these new steps: 1. Turn off and then turn on the Smarther AC. Wait a few seconds and start the installation from the product settings: Menu, "Manage my home", Select a room, Configure my remote control. 2. If step 1 does not work, please reset your product and reinstall it. To do this: - Delete your product from Home + Control: “Manage my home”, “Room”, “Smarther AC”, “Settings”, “Delete” - Reset the product by pressing the button at the top right for 5 seconds until you hear a beep - Reinstall the product