The EASYKIT system, when installed in a single-family home with an EASYKIT Wifi with Netatmo and another non-connected monitor, must be powered by a single DIN power supply. The master-slave switch must be in the slave position on all monitors except one, the master monitor cannot be the connected/wifi one and it must be connected to the external control panel via two-wire technology.