How can we help?

What do the different LED colors and blinking patterns mean on the gateway and devices during installation?

Gateway

• Solid green: The Gateway network is open and ready for product installation

• Flashing green: The gateway is in Wi-Fi configuration mode

• Solid White short (Starting the product/ after full reset of the gateway): initial Boot

• Solid White continuous: stable connection between app and phone

• Orange, short blink (1 flash): Wi-Fi and HomeKit reset triggered (after 10s press).

• Solid orange: Full reset in progress (after 20s press).

• Blinking blue: A firmware update is in progress.

 

Devices

• Solid green: Zigbee network successfully opened or joined.

• Flashing green (only for wireless devices): Device joining the network (success = solid green, failure = solid red).

• Solid red: Device powered and searching for network.

• Purple/blue: disconnected from device, still connected to zigbee network.

 

Updated