How can we help?

Is it possible to change or even interchange the supplied cores with another Three-Phase Energy Meter with Netatmo ?

No, it is not possible to change or interchange the supplied measurement coils with another Three-Phase Energy Meter with Netatmo. The closed measurement coils provided with the three-phase energy meter are specifically calibrated and matched to the module they come with.

Reasons for Non-Interchangeability:

  • Calibration: Each set of coils is calibrated to work specifically with its corresponding energy meter module. Using a different set of coils can result in inaccurate measurements. 📏
  • Unique Identification: The cores and the module have a unique and identical code to ensure they are used together. This helps maintain the accuracy and reliability of the measurements. 🔒

For accurate and reliable power measurement, always use the measurement coils supplied with the Three-Phase Energy Meter with Netatmo. Interchanging them with another set is not recommended and could lead to incorrect readings.

Updated