How can we help?

What means the "Total (5)" product marking on the 5th input?

The "Total (5)" marking on the 5th input indicates that this input is used to measure the total electrical consumption. However, depending on the presence or absence of connection to the TIC (Transmission d'Information de la Consommation), this input can be used to measure the electrical consumption of a specific line.

ℹ️ Two scenarios are possible:

  • If the TIC is connected and functional, input 5 becomes a measuring line for a specific circuit. In this case, total consumption data is obtained directly from the TIC.
  • If the TIC is not connected, connect input 5 to the main circuit breaker. This allows measurement of the total electrical consumption using the associated current transformer.

🔧 This configuration offers great flexibility by adapting the measurement of electrical consumption according to the specific needs of the system.

Updated