How can we help?

Can I calibrate shutters in Home + Pro ?

For now, the shutters calibration has to be made in Home + Control and not in Home + Pro. But it is also possible to calibrate the shutters directly on the physical products by following these steps:

1. Simultaneously press the up and down buttons for 7 s.

2. The light flashes in orange.

3. Do not press any button on the product during this calibration procedure for about 5 min.

4. The light stops flashing, the calibration is complete.

 

Updated