Before switching from heating to cooling mode, check that your system is compatible and check that you have carried out all the operations on the system necessary to change mode. The switch from heating to cooling is performed by programming the temperature. In the Home+Control App, go to Settings and select "Schedules". Clicking on the name of the schedule opens a drop-down menu, where you can select "Cooling". Now you can create a new cooling program or activate an existing one. Consider that the switch from heating to cooling mode is performed for all thermostats connected in the house.
Updated