How can we help?

Why consumptions measured by the measure module do not appear in Home + Control?

Consumptions measured by the measure module may not appear immediately due to the presence of multiple measure modules or because it was recently installed.

  1. Presence of multiple measure modules:
    • If the installation has multiple measure modules, it is necessary to keep only the one that measures the total consumption and remove the others.
       
  2. Recent installation:
    • If the measure module has just been installed, it needs time to properly measure all consumptions before they appear in Home + Control. This waiting period can be up to 24 hours after the module installation.