HOME+PROJECT can configure: max 30 rooms, max 50 objects per room. For each object it is possible to link max 50 local push buttons/contact interface.
HOME+PROJECT can configure: max 30 rooms, max 50 objects per room. For each object it is possible to link max 50 local push buttons/contact interface.
<%= block.description %>
<% } %><%= block.description %>
<% } %>