How can we help?

How do I restore the WiFi network on my Class 300 EOS? Example: after changing the WiFi password, changing the WiFi router or WiFi repeater...

The connection between the Classe 300 EOS and your WiFi line can be set from the device screen; select the Settings menu (gear) / Network The WiFi LED on your Classe 300 EOS will continue to flash red until the connection with the WiFi network is re-established, at which point the WiFi LED will turn off.