You can install the Classe 300 EOS on Bticino systems with Digital 8 and Analogue technology by adding specific interfaces. For more information, consult the technical guide You can configure the connection between the Classe 300 EOS and your Wi-Fi line from the device display, turn on the display, open the Settings menu (dial) / Network The Wi-Fi LED on your Classe 300 EOS will continue to flash red until the connection to the Wi-Fi network is reestablished; at the end of the operation, the Wifi LED will turn off.