How can we help?

How do I reset the WiFi network on my Class300 EOS? Example: after changing the WiFi password, changing the WiFi router or WiFi repeater...

You can set up the connection between the Classe 300 EOS and your WiFi from the device screen, turn on the screen and open the menu in Settings (wheel) / Network The wifi LED of the Classe 300 EOS will continue to flash red until the connection to the WiFi network is reestablished. The Wifi LED will turn off once this is complete.