How can we help?

How to install the wifi network in the Class 300 EOS?

You can configure the EOS Class 300 connection and the wifi connection with the power supply of the device: turn on the device, open the menu Settings (wiel) / Network The full connection with the WiFi network is established; The connection is now disconnected and the LED lamp is connected to the wifi connection.