The Home + Control App enables you to give access to your installation to your relatives. In order to configure that, please follow these steps:
1. Open the Home + Control App
2. Navigate to Settings and select Guests
3. Choose "Invite a user"
They will receive an e-mail inviting them to accept the invitation.
Once the application is downloaded, they will have access to your home via their smartphone.
Once invited, they will get exactly the same access rights than the person who invited them (for example, invite new users, or remove existing ones).
On the other hand, you can remove access by following these steps:
1. Click on the trash next to the account whose access you wish to remove
2. Click on Remove access to confirm
Additional options
You can also remove your own acces to the home. If the home’s creator removes his own access, the guests still keeps theirs.
In the same way, if you are an installer and you remove your own access to the home once installation and setup are completed, the home’s owner will be able to get the existing configuration by following the installation guide in his Home + Control App, when he moves in.
Updated