Skip to main content
Search
How can we help?
Search
Legrand Help Center
Classe 300EOS with Netatmo
Application Features
Application Features
What does the orange “charge has been discharged” banner mean?
How many smart automations can I create for MyHome setup via the Home + Control app?
What does the orange banner “This room is protected against humidity” mean?
Where can I adjust the fade in and fade out settings of a Dali2 lamp?
What can I do with a Dali2 lamp in Home + Control?
Can the MyHOME installation manage an energy meter?
How many smart notifications can I create for MyHome setup via the Home + Control app?
How can I identify an actuator in my installation if I cannot reach it?
Is it possible with Classe 300EOS to export the SCS address configuration of the installation?
Is it possible to calibrate the thermostats of the MyHome installation?
How can I view consumption and production graphs of my monitored lines?
Can I manage Dali2 lamps with Classe 300EOS?
How can I copy favorites from one Dali2 light to another in Home + Control?
How do I set up the energy meter?
What time measurement is used for sunrise and sunset conditions that I can use as a trigger and condition for scenes?
How many scenes can I create for the MyHome installation via the Home + Control app?
What functions can be configured with BT-F522, BT-F523 and BT-*4672N and other built-in products?
How many F422A can I add to an installation with Class 300EOS?
How do I adjust the charge control system?
Where can I set the humidity logic thresholds in the Class 300EOS?
What other gateway can I add to the MyHome installation?
What time measurement is used for sunrise and sunset conditions that I can use as a trigger for Home + Control scheduled actions?
How can I see the instantaneous consumption/production of my monitored lines?
How can I change the order of uploads?
What are the differences between F429D and F429G?
How can I add an object to the system?
Can I use an Eliot account to log in to Home + Project?
need to replace Class 300EOS, how can i do?
How many objects can I add in a Home + Control scene?
How do I invite other “guest” users to manage my installation?
Next
›
Last
»
<% var getColumnClasses = function(columnNumber) { var classNames = numberColumns === 'auto' ? 'col-auto' : 'col-12'; if (numberColumns >= 2) classNames += ' md:col-6'; if (numberColumns >= 3) classNames += ' lg:col-4'; if (numberColumns >= 4) classNames += ' xl:col-3'; return classNames; } %>
Browse the articles by selecting a topic
<% blocks.forEach(function(block, index) { %>
<% if (imageHeight) { %>
<% } %> <% if (block.name) { %>
<%= block.name %>
<% } %> <% if (block.description) { %>
<%= block.description %>
<% } %>
<% }) %>
Still can't find the answer to your questions?
<% blocks.forEach(function(block, index) { %>
<% if (imageHeight) { %>
<% } %>
<% if (block.name) { %>
<% if (block.html_url) { %>
<%= block.name %>
<% } else { %> <%= block.name %> <% } %>
<% } %> <% if (block.description) { %>
<%= block.description %>
<% } %>
<% }) %>
Categories
<% categories.forEach(function(category, index) { %>
<%= category.name %>
<%= partial('partial-article-list-sections', { id: 'category-' + category.id, parentId: '#sidebar-article-navigation', sections: category.sections, activeCategoryId: activeCategoryId, activeSectionId: activeSectionId, activeArticleId: activeArticleId, partial: partial }) %>
<% }); %>
<% var maxSections = 20 %>
Toggle navigation menu
<% categories.forEach(function(category, index) { %> <% if (category.id === activeCategoryId) {%>
<%= category.name %>
<%= partial('partial-section-list-sections', { parent: category, sections: category.sections, maxSections: maxSections, partial: partial }) %>
<% } %> <% }); %>
Categories
Categories
<% categories.forEach(function(category) { %>
<%= category.name %>
<% }); %>
<% if (sections.length) { %>
<% sections.forEach(function(section) { %>
<%= section.name %>
<%= partial('partial-article-list-sections', { id: 'section-' + section.id, parentId: '#' + id, sections: section.sections, activeCategoryId: activeCategoryId, activeSectionId: activeSectionId, activeArticleId: activeArticleId, partial: partial }) %> <% if (section.articles.length) { %>
<% section.articles.forEach(function(article) { %>
<%= article.title %>
<% }); %>
<% } %>
<% }); %>
<% } %>
<% if (sections.length) { %>
<% sections.slice(0, maxSections).forEach(function(section) { %>
<%= section.name %>
<%= partial('partial-section-list-sections', { parent: section, sections: section.sections, maxSections: maxSections, partial: partial }) %>
<% }); %> <% if (sections.length > maxSections) { %>
See more
<% } %>
<% } %>
Powered by Zendesk