How can we help?

How do I set up Google Assistant to control connected products in my home?

If you have a Google Home speaker, you can configure it via the "Google Home" application available on iPhone and Android. For more information, you can consult the following page on the Google support website. https://support.google.com/assistant If you do not have a speaker, simply download the "Google Assistant" application on your smartphone, available on the App Store for iOS and Google Play for Android. First, you need to make sure that your installation is properly connected to the Internet. You can check this by checking that the connected installation is accessible from the Home + Control app: 1- Launch the "Google Assistant" application and select the blue button in the top right corner of the page. 2- Go to settings and select "Home control" in the list of services. 3- Click on "Add devices" and select the "Home + Control" service. 4- Enter the email address and password of your Legrand - Netatmo - Bticino account, select "Connect". After synchronization, the list of products configured in Home + Control appears. 5- You can now, if you wish, associate each connected product with a room. Select the pen icon to edit each product. 6- Select a room from the list or customize a new one. 7- Repeat the operation until all the products in the installation are associated with a room. Google Assistant is configured, you can now control the heating with voice control.