The Connected Dry-Contact is able to measure the energy consumption of the appliance through its closed measurement coil. It is able to measure single-phase line up to 80A. Finally, It also allows to remotely-control and remotely report the device which is cabled to.