Alexa voice control can only be set up with a 2.4 GHz home Wi-Fi network that does not have port filtering. It is compatible with 802.11 b/g/n Wi-Fi standards if the network security settings are set to WEP, WPA, or WPA2 Personal.
Alexa voice control can only be set up with a 2.4 GHz home Wi-Fi network that does not have port filtering. It is compatible with 802.11 b/g/n Wi-Fi standards if the network security settings are set to WEP, WPA, or WPA2 Personal.
<%= block.description %>
<% } %><%= block.description %>
<% } %>