Yes, follow the full control setup and enable or disable "proximity" in the setup page. If you enable it, you can choose between 3 distance levels: min, medium, max.
Yes, follow the full control setup and enable or disable "proximity" in the setup page. If you enable it, you can choose between 3 distance levels: min, medium, max.
<%= block.description %>
<% } %><%= block.description %>
<% } %>