Yes, follow the full order setup and in the settings page enable or disable the "proximity sensor". If you enable it, you can choose between 3 distance levels: min, medium or max.
Yes, follow the full order setup and in the settings page enable or disable the "proximity sensor". If you enable it, you can choose between 3 distance levels: min, medium or max.
<%= block.description %>
<% } %><%= block.description %>
<% } %>