Yes, when setting up the fully digital control, enable or disable the "proximity" option on the settings page. If you enable the option, you can choose between 3 distances: min, average and max.
Yes, when setting up the fully digital control, enable or disable the "proximity" option on the settings page. If you enable the option, you can choose between 3 distances: min, average and max.
<%= block.description %>
<% } %><%= block.description %>
<% } %>