How can we help?

How do I set up my Google Assistant to control my home's connected products?

If you have a Google Home speaker, you can set it up via your ;Google Home ; app, available on iPhone and Android. For more information, you can visit the following page on the Google support site. https://support.google.com/assistant. If you don't have a speaker, simply download the ;Google Assistant ; app on your smartphone, available on the App Store for iOS and on Google Play for Android. First, you need to make sure that your ;...with Netatmo ; installation is connected to the Internet. You can check this by checking that your connected installation is accessible from the Home + Control application. Proceed as follows: 1- Launch your ;Google Assistant ; app and select the blue button at the top right of the page. 2- Go to settings and select ;Home Control ; from the list of services. 3- Click on ;Add devices ; and select the application ;Home + Control; 4- Enter the email address and password of your Legrand - Netatmo - Bticino account, select ;Connect;. After synchronization, the list of products configured in Home + Control is displayed. 5- You can now, if you wish, associate each connected product with a room. Select the pen icon to modify each product. 6- Select a room from the list or customize a new one. 7- Repeat the operation until all the products in your installation are associated with a room. Your Google Assistant is configured, you can now control your heating using voice control.