How can we help?

In the case of installations with Smarther AC with Netatmo and IR emitters, what should I manage via the physical interface of the thermostat?

In an installation with Smarther AC with Netatmo and one (or more) IR emitters, the commands of the physical device act as a room control: I send the control to all the air conditioners in the same room as Smarther AC. Note: if you want to manually manage by Smarther AC with Netatmo all the IR emitters that are located in different rooms, you must install a Smarther AC in each room.