How can we help?

Is it possible to turn off my Smarther air conditioner with Netatmo manually or via the app?

It is not possible to turn off your thermostat without cutting it directly in your electrical panel. If you wish to disable the temperature regulation, please follow the instructions below. When your home is in cooling mode: You can activate the OFF mode (without end date) by increasing the setpoint above the maximum available level. You can also turn off your thermostat directly in the H+C app: - for the single thermostat, by selecting the dedicated close product command (in the dashboard) - at the home level To do this, click on the menu at the bottom of the home page, then select the temperature programming section and click on OFF to activate the mode and set an end date if necessary. When your home is in heating mode: You can activate the OFF mode (without end date) by decreasing the setpoint below the minimum available level. You can also turn off your thermostat directly in the app H+C: - for the simple thermostat, by selecting the dedicated command close the product control close the product (in the dashboard) - at the home page To do this, click on the menu at the bottom of the home page, then select the temperature programming section and click OFF to activate the mode and set an end date if necessary.