No, it is not mandatory. The choice depends on the current (mA) available on the BUS and the distances. The maximum consumption of the Linea 5000 is 560 mA and the minimum voltage required is 23 VDC. The maximum distance without local power supply is 65 m. If necessary, it is possible to use the reference 346020 as a local power supply.
Updated