How can we help?

What is the difference between automatic and manual sync?

Automatic synchronization allows the following changes (both via Bluetooth and remote control): - adding/removing/modifying residents of an existing apartment - adding/removing/modifying badges - adding/removing/modifying access codes - adding/removing/modifying staff users - adding/removing/modifying messages Simply send the previous changes to a Linea 5000, which will automatically send them to the other devices thanks to propagation via SCS. Manual synchronization allows the following changes (structural changes, via Bluetooth only): - adding/removing/modifying apartments - adding/removing/modifying gates - adding/deleting/modifying tables All changes must be pushed manually to each device, one at a time.

Updated