How can we help?

I haven't configured my EOS Class 300, what do you think?

Open the Home + Security app and select Install new products in Settings. Follow the instructions. Make sure your smartphone is connected to a 2.4 GHz network. The EOS 300 series model is not compatible with 5 GHz networks. If you are using an iOS device and you receive the error message “Unable to add accessory”, put your iOS device in airplane mode for more than 30 seconds, turn off airplane mode, and restart the installation. If you are using an Android device, make sure that no ad blocking apps are enabled on your device. If so, disable the adblocker application when installing the Classe 300 EOS. If you want to install the Classe 300 EOS on a Wi-Fi repeater: Make sure it does not have the same name (SSID) as the router. To check if the repeater is working properly, try installing the Classe 300 EOS directly on the router (by changing the network to which the smartphone is also connected).