How can we help?

When you press the button on the Class 300 EOS to protect the bracelet, do you have to repeat it without wanting the order to have the bracelet?

English: If, when pressing the lock opening button, the corresponding LED flashes several times without sending a command to the lock, the Classe 300 EOS is in Secure Lock mode, in which the buttons are only active when there is an audio/video connection between the videophone and the external door station. To deactivate Secure Lock mode: — Remove the Classe 300 EOS from the wall bracket. — Remove the green power supply terminal block. — Move the “Secure Lock Function” microswitch, located on the back of the videophone, to the right. — Reinsert the green power supply terminal block. — Reattach the videophone to the wall bracket. This operation must be carried out by an authorized person.