How can we help?

How many Class 100X can I have in a single apartment/house?

Only one Class 100X can be installed per dwelling. In dwellings with several video intercoms, it is possible to install 1 Class 100X and up to 2/4 Class 100 in the same dwelling; for more information, consult the technical guide.