NO BUT It is possible to use the same Internet cables to connect two or more EASYKIT Wifi With Netatmo from different apartments; each EASYKIT Wifi With Netatmo must be connected to a different WiFi access point, each with its own different SSID
NO BUT It is possible to use the same Internet cables to connect two or more EASYKIT Wifi With Netatmo from different apartments; each EASYKIT Wifi With Netatmo must be connected to a different WiFi access point, each with its own different SSID
<%= block.description %>
<% } %><%= block.description %>
<% } %>