The WiFi network to which the EASYKIT Wifi Avec Netatmois is connected must be of type 2.4GHz 802.11 b/g/n. 5GHz type networks are not compatible.
The WiFi network to which the EASYKIT Wifi Avec Netatmois is connected must be of type 2.4GHz 802.11 b/g/n. 5GHz type networks are not compatible.
<%= block.description %>
<% } %><%= block.description %>
<% } %>