Skip to main content
Search
How can we help?
Search
Legrand Help Center
F460
F460
App Features
Can I use an Eliot account to login in Home + Project?
I need to replace a device on the installation, how can I do that?
Connecting to my Wi-Fi network
If HOME+PROJECT application ask me the "INSTALLER CODE", where I can find?
Which are the limits of a MyHome installation? How many rooms and object it's possible manage in the same project?
With F460 can I integrate the temperature central unit BT-3550?
Is it possible use HOME+PROJECT remotely?
Can I complete the commissioning without Internet connection?
Configuration
Which measure of time is used for sunrise and sunset condition that I can use as trigger and condition for scenes?
Which functions can be configured with the BT-F522, BT-F523 and BT-*4672N and the other flush mounted products?
How can I set the load control system?
How can I configure the energy meter?
Can MyHOME installation manage an energy meter?
Where I can set the thresholds of humidity logic in the F460?
See all 17 articles
Start my connected project
How can I update the firmware of F460?
Is it possible to test the installation through the app Home + Project?
Can I install a touch screen on the installation to manage all objects connected on the system?
What about compatibility with vocal assistant?
Can I manage installations with F460 with physical configurators?
Is it possible manage a LIFX on MyHOME installation?
See all 9 articles
Troubleshooting
What can I do with the copy&paste function of Home + Project?
How can I connect to F460 ?
With F460 can I integrate the driver manager BT-F459?
Can I create a scenarios for lights and shutters linked to Sunrise and Sunset condition?
How many scenarios it's possible create by HOME+PROJECT?
Do I have to pay for the HOME+PROJECT application to manage installations?
Installing my connected products
Which are a limits of a scenario? How many start condition and actions each scenario could manage?
Which is the automation addresses limit for MyHome installation?
Is it possible manage a Philips HUE on MyHOME installation?
Can I configure more than one house with the HOME+PROJECT application?
Is it possible to create group and general commands in Home + Project?
<% var getColumnClasses = function(columnNumber) { var classNames = numberColumns === 'auto' ? 'col-auto' : 'col-12'; if (numberColumns >= 2) classNames += ' md:col-6'; if (numberColumns >= 3) classNames += ' lg:col-4'; if (numberColumns >= 4) classNames += ' xl:col-3'; return classNames; } %>
Browse the articles by selecting a topic
<% blocks.forEach(function(block, index) { %>
<% if (imageHeight) { %>
<% } %> <% if (block.name) { %>
<%= block.name %>
<% } %> <% if (block.description) { %>
<%= block.description %>
<% } %>
<% }) %>
Still can't find the answer to your questions?
<% blocks.forEach(function(block, index) { %>
<% if (imageHeight) { %>
<% } %>
<% if (block.name) { %>
<% if (block.html_url) { %>
<%= block.name %>
<% } else { %> <%= block.name %> <% } %>
<% } %> <% if (block.description) { %>
<%= block.description %>
<% } %>
<% }) %>
Categories
<% categories.forEach(function(category, index) { %>
<%= category.name %>
<%= partial('partial-article-list-sections', { id: 'category-' + category.id, parentId: '#sidebar-article-navigation', sections: category.sections, activeCategoryId: activeCategoryId, activeSectionId: activeSectionId, activeArticleId: activeArticleId, partial: partial }) %>
<% }); %>
<% var maxSections = 20 %>
Toggle navigation menu
<% categories.forEach(function(category, index) { %> <% if (category.id === activeCategoryId) {%>
<%= category.name %>
<%= partial('partial-section-list-sections', { parent: category, sections: category.sections, maxSections: maxSections, partial: partial }) %>
<% } %> <% }); %>
Categories
Categories
<% categories.forEach(function(category) { %>
<%= category.name %>
<% }); %>
<% if (sections.length) { %>
<% sections.forEach(function(section) { %>
<%= section.name %>
<%= partial('partial-article-list-sections', { id: 'section-' + section.id, parentId: '#' + id, sections: section.sections, activeCategoryId: activeCategoryId, activeSectionId: activeSectionId, activeArticleId: activeArticleId, partial: partial }) %> <% if (section.articles.length) { %>
<% section.articles.forEach(function(article) { %>
<%= article.title %>
<% }); %>
<% } %>
<% }); %>
<% } %>
<% if (sections.length) { %>
<% sections.slice(0, maxSections).forEach(function(section) { %>
<%= section.name %>
<%= partial('partial-section-list-sections', { parent: section, sections: section.sections, maxSections: maxSections, partial: partial }) %>
<% }); %> <% if (sections.length > maxSections) { %>
See more
<% } %>
<% } %>
Powered by Zendesk