Skip to main content
Search
How can we help?
Search
Legrand Help Center
MyHome
MyHome
Application Features
Can I control more than one home with the Home + Control application?
Can installer manage my installation?
Is there a limit to the number of accounts which can be invited to share the same installation?
What if I have to change in Home + Control between heating and cooling mode?
Can I modify one scenario created by my installer?
How can I create programs for fan coil and towel rail?
See all 59 articles
Start my connected project
Is it possible manage a LIFX on F460 installation?
Do you have to pay for the Home + Control application to control my installation?
Is it possible manage a Philips HUE on F460?
What kind of network do I need in my apartament to install F460?
Could Home + Control manage third party system?
Which are the limits of a scenario?
See all 16 articles
Safety and conditions of use
How my connected installation data are used?
Are my data protected during communication transit through the cloud?
How my connected installation data are used?
Are my data protected during communication transit through the cloud?
Use of connected products
If there is an Internet outage in my home, will my MyHOME installation continue to work?
If there is an Internet outage in my home, will my MyHOME installation continue to work?
Using my connected products
Can I modify a functionalities of a local command present in my home? For example invert a 2 pushbuttons on the same comand?
If there is a power cut, will my MyHOME installation still work? Is there a memory function in all devices?
Will all the features available on MyHOMEServer1 be available on Classe 300EOS with Netatmo?
If there is a power cut, will my MyHOME installation still work? Is there a memory function in all devices?
Can I modify a functionalities of a local command present in my home? For example invert a 2 pushbuttons on the same comand?
Troubleshooting
I need to replace a device, how can I do that?
I need to replace a device, how can I do that?
Burglar alarm system
How many burglar alarm system central units I can have on the same network?
How can I create smart home scenarios including the burglar alarm system?
I need to change the PIN code of the burglar alarm system, how can I?
I cannot start an Alarm's scenarios of the burglar alarm system
How can I include or exclude a sensor?
Where can I see eventual failures of the burglar alarm system?
See all 15 articles
<% var getColumnClasses = function(columnNumber) { var classNames = numberColumns === 'auto' ? 'col-auto' : 'col-12'; if (numberColumns >= 2) classNames += ' md:col-6'; if (numberColumns >= 3) classNames += ' lg:col-4'; if (numberColumns >= 4) classNames += ' xl:col-3'; return classNames; } %>
Browse the articles by selecting a topic
<% blocks.forEach(function(block, index) { %>
<% if (imageHeight) { %>
<% } %> <% if (block.name) { %>
<%= block.name %>
<% } %> <% if (block.description) { %>
<%= block.description %>
<% } %>
<% }) %>
Still can't find the answer to your questions?
<% blocks.forEach(function(block, index) { %>
<% if (imageHeight) { %>
<% } %>
<% if (block.name) { %>
<% if (block.html_url) { %>
<%= block.name %>
<% } else { %> <%= block.name %> <% } %>
<% } %> <% if (block.description) { %>
<%= block.description %>
<% } %>
<% }) %>
Categories
<% categories.forEach(function(category, index) { %>
<%= category.name %>
<%= partial('partial-article-list-sections', { id: 'category-' + category.id, parentId: '#sidebar-article-navigation', sections: category.sections, activeCategoryId: activeCategoryId, activeSectionId: activeSectionId, activeArticleId: activeArticleId, partial: partial }) %>
<% }); %>
<% var maxSections = 20 %>
Toggle navigation menu
<% categories.forEach(function(category, index) { %> <% if (category.id === activeCategoryId) {%>
<%= category.name %>
<%= partial('partial-section-list-sections', { parent: category, sections: category.sections, maxSections: maxSections, partial: partial }) %>
<% } %> <% }); %>
Categories
Categories
<% categories.forEach(function(category) { %>
<%= category.name %>
<% }); %>
<% if (sections.length) { %>
<% sections.forEach(function(section) { %>
<%= section.name %>
<%= partial('partial-article-list-sections', { id: 'section-' + section.id, parentId: '#' + id, sections: section.sections, activeCategoryId: activeCategoryId, activeSectionId: activeSectionId, activeArticleId: activeArticleId, partial: partial }) %> <% if (section.articles.length) { %>
<% section.articles.forEach(function(article) { %>
<%= article.title %>
<% }); %>
<% } %>
<% }); %>
<% } %>
<% if (sections.length) { %>
<% sections.slice(0, maxSections).forEach(function(section) { %>
<%= section.name %>
<%= partial('partial-section-list-sections', { parent: section, sections: section.sections, maxSections: maxSections, partial: partial }) %>
<% }); %> <% if (sections.length > maxSections) { %>
See more
<% } %>
<% } %>
Powered by Zendesk