In the Apple store, the application is always visible, but during installation a blocking pop-up explains that it is not compatible with the smartphone In the Google Play Store, the application is not visible if the smartphone is not compatible
In the Apple store, the application is always visible, but during installation a blocking pop-up explains that it is not compatible with the smartphone In the Google Play Store, the application is not visible if the smartphone is not compatible
<%= block.description %>
<% } %><%= block.description %>
<% } %>