The WiFi network to which the Classe 300EOS with Netatmo is connected must be of the 2.4 GHz 802.11 b/g/n type. 5 GHz type networks are not compatible.
The WiFi network to which the Classe 300EOS with Netatmo is connected must be of the 2.4 GHz 802.11 b/g/n type. 5 GHz type networks are not compatible.
<%= block.description %>
<% } %><%= block.description %>
<% } %>