It is possible to have 2 Classe 300 EOS per home. In apartments equipped with several videophones, it is possible to install on the same call 2 Classe 300EOS and up to 3 Classe 100x; for more information, consult the technical guide.
It is possible to have 2 Classe 300 EOS per home. In apartments equipped with several videophones, it is possible to install on the same call 2 Classe 300EOS and up to 3 Classe 100x; for more information, consult the technical guide.
<%= block.description %>
<% } %><%= block.description %>
<% } %>