"It is possible to have only one EOS Class 300 per dwelling. In apartments with multiple video door entry systems, it is possible to install 1 Class 100x and up to 4 EOS Class 300 on the same call; for more information, see the technical guide. "
"It is possible to have only one EOS Class 300 per dwelling. In apartments with multiple video door entry systems, it is possible to install 1 Class 100x and up to 4 EOS Class 300 on the same call; for more information, see the technical guide. "
<%= block.description %>
<% } %><%= block.description %>
<% } %>