How can we help?

Can I replace an existing Bticino 2-wire video intercom?

It is possible to replace the existing videophone with a Class 100X: - Single-family or two-family house: replacement without modifying the installation wiring - Collective house: depending on the characteristics of your installation, it may be sufficient to replace the videophone or it may be necessary to add an additional power supply, code 346020. For the sizing of collective systems, please refer to the general installation rules in the 2-wire instructions.